Digital Isolation Products for Brushless DC Motors
Isolation
is critical to protect both an electronics system and the user from potentially hazardous
voltages, or where a high level of electrical isolation between electronics systems is
necessary. Digital isolators are known for their speed of data transmission,
high level of magnetic immunity, and long life expectancy. Used in combination with isolated
power supplies, these devices protect circuits from high voltages, prevent current flow between
remote system grounds, and avoid the creation of current loops. Digital
isolators can be used to implement isolation in designs without the cost, size,
power, performance, and reliability constraints found with optocouplers.
Featured Suppliers
USB Receptacles for Brushless DC Motors
USB plugs
and receptacles are designed to reduce human error by their unique shape; they
fit together in only one way. USB plugs and receptacles are Type A (connecting to hosts or hubs)
or Type B (connecting to devices) and are available 3 sizes: standard, mini, and micro.
Type A plugs always face upstream, Type B faces downstream.
USB is used in many applications covering all areas of electronics that require
communication, but more commonly with devices that need fast or easy connections for interaction
with computers. Since USB provides a small charging current as well, it is becoming a de facto
standard for charging portable devices.
Featured Suppliers
Switches for Brushless DC Motors
Switches are
devices that provide manual input or control for equipment, a device, or a process. Switches
serve many purposes, provide immediate emergency control, local control, or indication; and are
available in many formats, shapes, sizes, and colors. Switches and buttons are important in
everyday use from light switches or buttons to automatic switches that shut off
a motor when an attached gate has fully shut.
Featured Suppliers
DC / DC Regulators for Brushless DC Motors
DC / DC
regulators are circuits that convert DC voltage from one level to
another and maintain that voltage to a constant level. Electronic systems often have several
sub-circuits, each with its own voltage level requirement that may be higher or lower than the
main power supply. Step-up converters or regulators boost a voltage to a higher level. Step-down
converters or regulators lower (or “buck”) a voltage to a lower level. DC / DC
converters and controllers can also be used for the same purpose,
but may offer options such as multiple softstart levels, undervoltage lockout, protection
against overvoltage and undervoltage, and programmable short-circuit protection. All of these
devices are considered to be in the same category of integrated chips, typically categorized as
power management devices.
Featured Suppliers
RS-485 Products for Brushless DC Motors
RS-485 is an
electrical-only standard, in contrast to complete interface standards which define physical,
functional, and electrical specifications. RS-485 signaling can be used with many protocols such
as Profibus, Interbus, Modbus, or BACnet, depending on the requirements of the end user.
Sometimes controller area network (CAN) or EtherNet are preferred for network requirements.
RS-485 has a 10 Mbps maximum data rate (@ 40 feet) and a 4000 foot maximum
cable length (@100 kbps.) RS-485 is robust and well suited for long distance
networking in noisy environment.
Featured Suppliers
CAN Products for Brushless DC Motors
CAN is an acronym for
Controller Area Network and refers to a fault-tolerant communications protocol
that is flexible for system design, supports multiple network topologies, and has become a de
facto standard for high integrity serial communications in industrial and automotive embedded
applications. In a CAN network, several short pieces of data like a motor’s run
status, temperature, or RPM is broadcast over the entire network at up to 1 megabit per second
(Mbps.) CAN is meant for applications that have to report and consume numerous but small pieces
of data consistently among nodes and has the ability to self-diagnose and repair data errors.
CAN is well-suited to environments with machinery, since CAN is designed to be
reliable in rugged environments that include interference or introduce noise. CAN is also
well-suited to the transportation industry.
Featured Suppliers
USB Products for Brushless DC Motors
USB is a standard
connection interface between computers and digital devices. A USB transceiver
is a physical layer device that prepares data for transmission and then sends to, and receives
data from, another transceiver. The transceiver detects connection and provides the low level
USB protocol and signaling. The term "transceiver" indicates an implementation of both transmit
and receive functions. It transmits and receives, encodes and decodes data, provides error
indication, implements buffers to stage data until it can be managed, and adjusts for the clock
rate from the serial stream on the USB SuperSpeed bus to match that of the
“link layer” higher up on the communication stack.
Featured Suppliers
ESD Products for Brushless DC Motors
Electrostatic Discharge
(ESD) is a naturally occurring phenomenon. If you have ever been zapped by a
socks-wearing kid who has just discovered static charge build up, you have experienced ESD first
hand. ESD is like a miniature, localized lightning bolt caused by an electrical
discharge. ESD can have seriously damaging effects on an integrated chip or system and cause
poor performance or failure later on by merely weakening the circuits.
Featured Suppliers
LCD Displays for Brushless DC Motors
LCD means
"liquid crystal display." It is an electronically driven flat panel screen that
orients liquid crystals within the panel in a direction that blocks or
transmits light coming from behind the panel. LCDs are a low cost, energy efficient visual
display that can be controlled in segments or as individual pixels, in shades of black and gray
or in full color. LCDs have most commonly replaced bulky cathode ray tubes in
televisions and computers and are available in all sizes. Liquid crystals were first discovered
in 1888, but were first put into common use in the early 1970s as electronic digital-display
watches.
Featured Suppliers
Processors for Brushless DC Motors
The term
"processor" refers to an electronic device that performs computational
functions and carries out the instructions of a stored program. Other terms for processor are
microprocessor, central processing unit, and digital signal processor. Essentially, the
processor refers to "the brains of a computer."
Featured Suppliers
Drivers for Brushless DC Motors
Designers of power electronic
circuits must often drive power switches that feed DC, AC, or power signals to a variety of
workloads. Logic-level electronic circuits provide the driving signals. In general, however, the
power sources and their loads have reference levels different from that of the control circuitry
(ground). MOSFET selection begins by choosing devices that can handle the required current, then
giving careful consideration to thermal dissipation in high current applications.
Featured Suppliers
ADCs for Brushless DC Motors
An Analog-to-Digital
Converter (ADC or A/D converter) measures the
magnitude of an input analog signal and converts it to a digital number that is proportional to
the magnitude of the voltage or current. An ADC often converts signals collected from the
real-world to digital signals for processing. One of the more important specifications of an
ADC is the resolution that it offers, which is the number of discrete values
(represented in bits) that the ADC produces in relation to the analog signal it is converting.
The more bits, the higher the resolution. A higher resolution yields a more accurate
approximation of the analog input.
Featured Suppliers
Amplifiers - Current Sensing for Brushless DC Motors
Current sensing
amplifiers, also known as current-sense or current-shunt
amplifiers, measure electrical current. The voltage across a resistor in a current
path is directly proportional to that current, per Ohm's law. Thus, measuring current is highly
dependent upon the resistance for accuracy. Integrated circuits for current measurement are more
efficient, accurate, and are an overall lower cost solution over a discrete current-sensing
solution.
Featured Suppliers
Amplifiers - Precision for Brushless DC Motors
A precision
amplifier is used for sensors to preserve accuracy. It increases the amplitude of
weak signals it receives while introducing as little noise as possible so that the signal
transfers an accurate or precise measure of what it is sensing. Amplifiers have
enormous voltage gain, often use feedback of the output signal back to the input of the
amplifier to operate, and can be classified in different ways. An amplifier can be identified by
the device they are intended to drive (e.g., audio amplifier), the input that they are to
amplify (e.g. sensing amplifier), the frequency range of the signal (e.g., RF,
audio), and by the function that they perform (e.g. buffer amplifier, current-sensing
amplifier.)
Featured Suppliers
Power Stage for Brushless DC Motors
Some applications must feed high
levels of current and voltage to power heavy electrical loads. The power stage
is a circuit of electronically-controlled transistors that act as high current switches. In
applications powering heavy loads, the power stage is the driving force.
MOSFETs or IGBTs are commonly used in a "bridge" configuration
to drive motors. Selection for the power stage begins by choosing devices that can handle the
required current, and careful consideration must be given to thermal dissipation. MOSFETs and
IGBTs are transistors capable of withstanding the duty of switching high power signals, and mean
"metal–oxide–semiconductor field-effect transistor" and "insulated gate bipolar transistor",
respectively.
Featured Suppliers
Temp Sensors for Brushless DC Motors
A temperature sensor
is a device that measures cold or heat as a temperature or temperature gradient. Many
applications require some implementation of temperature sensing and measurement. For motors, the
operating temperature inside the case is monitored by the processor and set to alarm or shut
down at temperatures higher than the normal operating temperature of the motor. If a motor runs
at too high of a temperature for too long, it can reduce the life of the motor.
Operating temperature is an indication of the general operating health of the motor. Higher
temperatures inside the motor case can mean too high of a load is placed on the motor, since as
load increases, motor current consumption increases to meet the load requirements.
Featured Suppliers
Hall Effect Sensors for Brushless DC Motors
Hall Effect
sensors are magnetically biased transducers that vary output voltage or current
in response to changes in a magnetic field. Hall Effect sensors can be designed to sense rotary
movement of a motor shaft. The rotation of the motor shaft changes the IC's position with
respect to the magnets, and thus detects the change in flux density. The output of the IC is
converted to a linear output over 90 degrees of shaft travel. The Hall Effect
sensor gets its name from Edwin Hall, who, in 1879 discovered that a voltage
difference can be produced across an electrical conductor where the magnetic field is
perpendicular to the direction of current flow.
Featured Suppliers
Encoders for Brushless DC Motors
An encoder, when
used with motors, is an electro-mechanical apparatus that translates the angular position of the
shaft of the motor into an electronic signal that a processor can understand. The information is
then used to calculate and report on speed of the motor, distance, revolutions per minute (RPM)
or position, usually for the purpose of automatic feedback control, some kind of intervention,
or shutdown.
Featured Suppliers